cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h755xih6 bsdl file

Hafez
Associate

Hi All,

It will be much appreciated if i can get a hints on how to obtain bsdl file of 

stm32h755xih6

 

I download the bsdl files of the family en.stm32h7_bsdl . (in web indicate that it include stm32h755xih6) but in reality dont have. 

This IC have a 265 pins

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Hafez, to the community!

The STM32H755XIH6 is in a TFBGA240 package that has 25 additional GND pins. In the data sheet it is therefore also called TFBGA240+25. The BSDL you downloaded is the correct one, because the included BSD contains the meaningfully testable 240 pins, the 25 additional GND pins cannot be tested by boundary scan.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.