STM32H755 interrupt issue after secure boot (SBSFU)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-12-06 8:39 AM - edited 2024-12-09 8:07 AM
I have a firmware running on an STM32H755. All working fine until I added a secure bootloader to the firmware and now the firmware crashes when initialising TIM3.
My setup:
STM32H755 on custom board
SBSFU (1_Image)
Cubeprogrammer and CubeIDE.
I've pinpointed the exact line that the firmware crashes on to be:
- Moving the call to MX_TIM3_Init to different points in the function. Still fails at that point.
- Commenting out the offending line. Firmware runs past this point but I need the timer.
- Calling the initialise function as part of the UserApp that comes with SBSFU on a Nucleo board. This works.
- Disabling the interrupt first.
- Hardcoding the address of the TIM3 DIER register
- Checked Timer is not setup by SBSFU
Might be Friday brain, but I'm really not seeing how this is connected to me having moved the firmware up a flashbank to make room for SBSFU.
Any thoughts greatly appreciated
Edit 1:
This appears to be interrupt related. I have put an __disable_irq() around the MX_INIT_** block in my main function and can now progress through this. However, the code then fallsover when using DMA.
0x800ae08
<signal handler called>() at 0xffffffe9
Init_DMA2_Transfer_FixedLocation_To_Fixed_Dest() at CW2_DMA.c:208 0x2400040e
seFillMemory16() at CW2_13748_API_hcl_parallel16.h:744 0x8082cba
There's nothing to go in the status registers.
I've check SP, LR and PC.
sp 0x2401ff48
lr 0x8087c05 (Hex)
pc 0x2400040e <Init_DMA2_Transfer_FixedLocation_To_Fixed_Dest+42>
Any tips on debugging the route to the top two items on my stack would probably be a big help in getting to the bottom of this.
- Labels:
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-12-10 2:12 AM
Turns out that the 0x800ae08 address is in the bootloader's vector table. While the user application firmware knows where it's vector is the hardware doesn't.
A solution is to update the beginning of main to:
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
extern const uint32_t g_pfnVectors[];
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
SCB->VTOR = (uint32_t)g_pfnVectors; // Set the vector table base address
/* USER CODE END 1 */
// Rest of program...
}
However, it seems like this is something that secure boot should be doing when loading the application so I need to dig around on that side.