cancel
Showing results for 
Search instead for 
Did you mean: 

stm32H753 vs stm32H733

MFäh.1
Associate II

Hi 

I just wanted to ask which of the two processors is actually more powerful. The H733 seems faster, but according to Google AI, the H753 offers better performance :). What’s your take on it?

 

Thank you

BR 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

According to objective facts, the H733 is faster and has a larger cache. It will therefore run code faster. I would call that more powerful.

H753: 

  • 480 MHz fCPU/, 2424 CoreMark /1027 DMIPS executing from Flash memory

H733: 

  • 550 MHz fCPU, 2778 CoreMark /1177 DMIPS executing from Flash memory
If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

According to objective facts, the H733 is faster and has a larger cache. It will therefore run code faster. I would call that more powerful.

H753: 

  • 480 MHz fCPU/, 2424 CoreMark /1027 DMIPS executing from Flash memory

H733: 

  • 550 MHz fCPU, 2778 CoreMark /1177 DMIPS executing from Flash memory
If you feel a post has answered your question, please click "Accept as Solution".

Thank you!