Skip to main content
Ivo
Associate II
July 21, 2021
Question

STM32H753 Unable to transmit CAN frames

  • July 21, 2021
  • 2 replies
  • 1328 views

I'm trying standard CAN communication from a STM32H743 Nucleo board, with an MCP2551 CAN transceiver connected to PA11/PA12. However, I'm not able to transmit anything.

With this same transceiver circuit, I am able to transmit CAN frames when connected to the CAN-FD interface of a NUCLEO-G474RE board, and with the CAN interface of a NUCLEO-F429ZI board.

- After HAL_FDCAN_Start, HAL_FDCAN_GetProtocolStatus returns:

     Activity: 0x0

      BusOff: 0x0

  LastErrorCode: 0x7

ProtocolException: 0x0

     TDCvalue: 0x0

- Starting with the second HAL_FDCAN_AddMessageToTxFifoQ() invocation, HAL_ERROR is returned, with HAL_FDCAN_GetProtocolStatus returning

     Activity: 0x0

      BusOff: 0x1

  LastErrorCode: 0x5

ProtocolException: 0x0

     TDCvalue: 0x0

- No errors reported by HAL_FDCAN_AddMessageToTxFifoQ() when testing with internal or external loopback mode.

- During all of these, no activity is seen on PA11/PA12 - both pins stay high

It seems like I'm missing a step to enable the CAN interface on PA11/12, but I'm not sure what to try next.

stm32h7xx_hal_map.c:

void HAL_MspInit(void)
{
 __HAL_RCC_SYSCFG_CLK_ENABLE();
}
void HAL_FDCAN_MspInit(FDCAN_HandleTypeDef* hfdcan)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(hfdcan->Instance==FDCAN1)
 {
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_FDCAN;
 PeriphClkInitStruct.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 __HAL_RCC_FDCAN_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**FDCAN1 GPIO Configuration
 PA11 ------> FDCAN1_RX
 PA12 ------> FDCAN1_TX
 */
 GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF9_FDCAN1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 }
}

main.c:

FDCAN_HandleTypeDef hfdcan1;
UART_HandleTypeDef huart3;
FDCAN_TxHeaderTypeDef TxHeader;
uint8_t TxData[] = {0x10, 0x32, 0x54, 0x76, 0x98, 0x00, 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x99, 0x00};
:
int main(void)
{
 SCB_EnableICache();
 SCB_EnableDCache();
 
 HAL_Init();
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_FDCAN1_Init();
 MX_USART3_UART_Init();
 
 HAL_StatusTypeDef rc;
 
 TxHeader.Identifier = 0x111;
 TxHeader.IdType = FDCAN_STANDARD_ID;
 TxHeader.TxFrameType = FDCAN_DATA_FRAME;
 TxHeader.DataLength = FDCAN_DLC_BYTES_8;
 TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
 TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
 TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
 TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
 TxHeader.MessageMarker = 0;
 
 FDCAN_ClkCalUnitTypeDef ClkCalUnit_FDCAN1;
 ClkCalUnit_FDCAN1.ClockCalibration = FDCAN_CLOCK_CALIBRATION_DISABLE;
 ClkCalUnit_FDCAN1.ClockDivider = FDCAN_CLOCK_DIV10;
 HAL_FDCAN_ConfigClockCalibration(&hfdcan1, &ClkCalUnit_FDCAN1);
 
 HAL_FDCAN_Start(&hfdcan1);
 
 while (1)
 {
 HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, &TxData[0]);
 HAL_Delay(1000);
 }
}
 
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
 __HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 24;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}
 
static void MX_FDCAN1_Init(void)
{
 hfdcan1.Instance = FDCAN1;
 hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan1.Init.AutoRetransmission = ENABLE;
 hfdcan1.Init.TransmitPause = DISABLE;
 hfdcan1.Init.ProtocolException = ENABLE;
 hfdcan1.Init.NominalPrescaler = 6;
 hfdcan1.Init.NominalSyncJumpWidth = 1;
 hfdcan1.Init.NominalTimeSeg1 = 55;
 hfdcan1.Init.NominalTimeSeg2 = 8;
 hfdcan1.Init.DataPrescaler = 1;
 hfdcan1.Init.DataSyncJumpWidth = 1;
 hfdcan1.Init.DataTimeSeg1 = 1;
 hfdcan1.Init.DataTimeSeg2 = 1;
 hfdcan1.Init.MessageRAMOffset = 0;
 hfdcan1.Init.StdFiltersNbr = 0;
 hfdcan1.Init.ExtFiltersNbr = 0;
 hfdcan1.Init.RxFifo0ElmtsNbr = 0;
 hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.RxFifo1ElmtsNbr = 0;
 hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.RxBuffersNbr = 0;
 hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.TxEventsNbr = 0;
 hfdcan1.Init.TxBuffersNbr = 0;
 hfdcan1.Init.TxFifoQueueElmtsNbr = 2;
 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }
}

This topic has been closed for replies.

2 replies

SKacp.1
Associate
July 21, 2021

Hi,

Please see my example for STM32 NUCLEO H743ZI2. Maybe it help You.

Best regards,

Slawek

Ivo
IvoAuthor
Associate II
July 22, 2021

Thanks Slawek. Unfortunately with your project I'm also getting transmission failures.

I assume it works for you; would you mind telling me which CAN transceiver you're using ?

Best regards,

Ivo.