cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753 CAN set up with both CAN-FD & CAN 2.0 frames

CZ_Home
Associate

Hi, I'm trying to configure an STM32H753 FDCAN peripheral to be compatible with both CAN-FD & CAN 2.0 frames, in both the Tx & Rx directions.

 

How should I configure the FD-CAN peripheral to achieve this? I've been through he RM0433 document as best I can and am struggling to find this information.

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

1- If you configure the peripheral in FDCAN frame format:

hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS

And you can send Classic CAN frames by setting the Tx header:

TxHeader.FDFormat = FDCAN_CLASSIC_CAN;

2- But if you intend to send FDCAN frames to CAN2.0 CAN nodes, this is not possible.

From this paper: Hybridization of CAN and CAN FD networks

"While CAN FD controllers can interpret and transmit both CAN FD and Classical CAN messages, Classical CAN controllers will report CAN FD messages as an error. This mandates a strict separation of CAN FD and Classical CAN networks"

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Karl Yamashita
Principal

Are you trying to send messages to FDCAN and CAN 2.0B nodes on the same bus? 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

mƎALLEm
ST Employee

Hello,

1- If you configure the peripheral in FDCAN frame format:

hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS

And you can send Classic CAN frames by setting the Tx header:

TxHeader.FDFormat = FDCAN_CLASSIC_CAN;

2- But if you intend to send FDCAN frames to CAN2.0 CAN nodes, this is not possible.

From this paper: Hybridization of CAN and CAN FD networks

"While CAN FD controllers can interpret and transmit both CAN FD and Classical CAN messages, Classical CAN controllers will report CAN FD messages as an error. This mandates a strict separation of CAN FD and Classical CAN networks"

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.