cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747I-DISCO programming

GunkutA
Senior

Hello, I just got STM32H747I-DISCO board. I have stlink-2 and I guess I cannot program this board with stlink2. Do I need to get STLink-3 or STLink-4 in order to program this board? In the description it says: Board has a built in STLink-v3 inside of it. Does it meanI " do not need an external programmer to program it"? If yes how will I do that without an external programmer. Thanks beforehand.

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13

Indeed it is Turkish, well I wish I was capable of to create that kind of autocorect plugin but here I am asking the most basic questions that could be asked.Yes, I fixed that but right now it says "Break at address "0xa05f0000" with no debug information available, or outside of program code." And that shows some assembly code in that. Maybe I am writing code to the wrong core? I don't know, I guess I should stick in the traditional STM32 MCU's. Even they are new for me.

P5 -> PI15 enable GPIOI with GPIO_PIN_15

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
GunkutA
Senior

.

Thank you, at least fixed compiler errors