2022-07-13 3:19 AM
Same question for pin PF14: can it be used as a single-ended ADC channel using ADC2_INP6 ?
The Cube does not indicate if these pins can be used as single-ended ADC channels.
Thank you.
Solved! Go to Solution.
2022-07-13 4:10 AM
Welcome, @BWolf.1, to the community!
We are sorry for any confusion this may cause, but IN6 (marked as INP6 in pinout view) is a single-ended input. It may be a little confusing that inputs like IN11 or IN14 are explicitly marked single-ended, which is just a left over from other derivatives in other packages of the same family where you can select differential and single-ended for the pin.
Summary: even if it is not explicitly marked single-ended on an ADC input - if it has no drop-down menu and can only be selected with a tick, then it is a single-ended input.
Does it answer your question?
Regards
/Peter
2022-07-13 4:10 AM
Welcome, @BWolf.1, to the community!
We are sorry for any confusion this may cause, but IN6 (marked as INP6 in pinout view) is a single-ended input. It may be a little confusing that inputs like IN11 or IN14 are explicitly marked single-ended, which is just a left over from other derivatives in other packages of the same family where you can select differential and single-ended for the pin.
Summary: even if it is not explicitly marked single-ended on an ADC input - if it has no drop-down menu and can only be selected with a tick, then it is a single-ended input.
Does it answer your question?
Regards
/Peter
2022-07-13 5:06 AM
Hi Peter,
That answers my question. Great!
Thank you very much.