2018-09-17 2:40 PM
Curious if anyone else encountered this: I work on a design using STM32H743XI silicon Y and DBGMCU seems to be completely dead. Reading any register returns 0 (so no REV_ID/DEV_ID). Writing to get 'timer freeze on debug' does not work either and reading back the written registers returns 0's.
The Errata does not mention anything like that.
I am aware that the Debugger is supposed to see DBGMCU at 0xE00E1000 and the CPU at 0x5C001000, but neither works.
Am I missing something ? - there is no RCC clock enabling for this class of MCUs... ; the ref manual lists DBGMCU->CR bits D1DBGCKEN and D3DBGCKEN, which are not dealt with in the standard HAL, but again trying to set them and re-read, I get back 0's...
Thanks.
2020-07-07 1:44 AM
As I mentioned above, this issue has been fixed in Keil 5.29. LL_DBGMCU_APB1_GRP1_FreezePeriph works for me.
2020-07-07 2:33 AM
Sorry, I missed your post on the topic. I'm gonna try the latest MDK version.
2023-07-05 1:52 AM - edited 2023-07-05 1:53 AM
Hello,
When the debugger is not connected and the clock gating feature is enable, the JTAG clock is automatically stop.
You must configure RCC_CKGAENR register to JTAGCKG clock gating disabled : the clock is always enabled then you can dump correctly REV_ID/DEV_ID @ 0x5C00100 address.
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.