Skip to main content
GS1
Senior III
March 1, 2018
Question

STM32H743: What is the purpose of pins FDCANn_TXFD/RXFD

  • March 1, 2018
  • 4 replies
  • 1460 views
Posted on March 01, 2018 at 14:39

We are currently setting up a project using STM32H743 and need to implement CAN / CAN-FD. When activating FDCAN1 or 2 in Cube as Mode 'FD', two additional checkboxes can be activated: Enable_FDCAN_TXFD and Enable_FDCAN_RXFD. When activating these, two additional RX/TX Pins are activated on the chip. What is the purpose of these Pins? Do we need to enable them to have CAN-FD work properly? I could not find any declaration of this. 

Thank you for any help.

Gabriele

    This topic has been closed for replies.

    4 replies

    ST Technical Moderator
    April 11, 2018
    Posted on April 11, 2018 at 18:23

    Hello

    Suchy.Gabriele

    ,

    Each FDCAN instance has 4 signals:

    CANn_RXFD/ CANn_TXFD are both outputs pins and they are used only for debug to show that the peripheral is in FDCAN mode.

    CANn_RX/ CANn_TX are used for CAN communicationas FDCAN Pins or classical CAN.

    Best Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Yan Rosh
    Associate II
    May 24, 2018
    Posted on May 24, 2018 at 09:21

    Hello,

    Sorry to reopen an old thready, but I just wanted to make sure what do you meant by debug outputs...

    We can use these pins to monitor the communication with a scope without probing the 'real' TX/RX lines?

    Are there any other functionality these pins provide?

    Can we use CANFD without these pins enabled?

    Thanks in advance,

    Yan

    ST Technical Moderator
    May 24, 2018
    Posted on May 24, 2018 at 09:50

    Hello

    yan.rosh

    ,

    CANn_RXFD/ CANn_TXFD are used only for debug and their usage is optional.

    We can use CANFD without these pins enabled.

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks