cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 UART configurations for non-standard baud rate

S.Kamath
Associate III

Hi,

I'm using STM32CubeMx to generate UART initialisation code for STM32H743 controller. I'm able to test UART communication for baud rate 3686400. 

I'm not able to make UART communication up & running when I changed baud rate to 4000000.

Is there other clock configurations to be changed to support UART baud rate of 4000000 ?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

The OVER8 allows for higher rates, but it's predicated on a) the APB clock source (perhaps alternate peripherals clock mappable) and b) integer divisibility by 8 or 16.

As speed increases the granularity of the divisor becomes predominant in the % clock error (actual vs desired). Send repetitive 0x55 ('U') character and scope signal to confirm timing.

Async serial is also not particularly robust. For tightly packed data consider 2 stop bits to aid resync. Going to want to use DMA to service UART.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I see below initialisation sequence for UART2. Do you suggest to change huart2.Init.OverSampling = UART_OVERSAMPLING_8 ?

------------------------------------------ UART2_init ---------------------

 huart2.Instance = USART2;

 huart2.Init.BaudRate = 4000000;

 huart2.Init.WordLength = UART_WORDLENGTH_8B;

 huart2.Init.StopBits = UART_STOPBITS_1;

 huart2.Init.Parity = UART_PARITY_NONE;

 huart2.Init.Mode = UART_MODE_TX_RX;

 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;

 huart2.Init.OverSampling = UART_OVERSAMPLING_16;

 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

 huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;

 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

 HAL_UART_Init(&huart2);

 HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8);

 HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8);

 HAL_UARTEx_DisableFifoMode(&huart2);