cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H735 - Error in initializing ST-Link device.Reason: (4) No device found on target.

HSamm.1
Associate II

I'm getting above error both of the two STM32H735G discovery boards that I have. On both boards ST-Link worked fine for some time until I unplugged the ST-Link USB connection while the MCU was stopped at a breakpoint. Afterwards it seems impossible to get them back to live. As soon as connected it turns on backlight and shows a white display. The reset button seems to have no effect. It is hard to believe that both boards have a similar hardware failure all a sudden.

I'm out of ideas, can anybody help?

10 REPLIES 10
HSamm.1
Associate II

Thanks, got it working via cubemx programmer.