cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 UHS cards problem not reaching full speed of W/R 48MBps/65MBps at second debugging session

Linas L
Senior II

Hello,

I made board with STM32H7 and i am running UHS example.

First time i always get 48MBps write and 65MBps read, but at the second debugging i get only 8MBps read/write speed, and i have to remouve card and insert it again to get back to that blistering speed. Any idea why ?

Also, does any one has fatfs working with UHS cards (with 1.8V tranciever)

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

The board I have with the transceiver has the Z Rev silicon so I'm not entirely sure the SDMMC is working, have other code working on X and Y Rev.

Not entirely sure the code I've seen would negotiate the mode switch properly.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

mine has rev Y.

Just in case will implement power cycle capability for sdcard

I've tried to do DDR on eMMC, and looked at code examples from ST, but wasn't able to make it function. The eMMC permits 3V signalling, and thus doesn't need a transceiver in this context. I've had eMMC solutions clocking at 52 MHz in 8-bit mode. And the parts did report as being DDR 3V capable.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..