cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 SPI ISSUE

MANISH
Associate II
Posted on April 06, 2018 at 16:43

Hai, Iam using the STM32H743VIT controller , We are using the spi4 in our board ,we generated the code using the cube mx nothing is coming(CLK and SIN)when transmit the data using the function ( HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout)). we configured the SPI to the 8 bit mode.But with the same configuration the SPI2 is working fine.

Thank you

Best regards

Maheshwar.

#uphill-skiing #stm32h7-spi-sync #stm32h7 #spi

Note: this post was migrated and contained many threaded conversations, some content may be missing.
10 REPLIES 10
laszpar
Associate II

Is there any progress of this issue?

Maybe I have the same problem:

https://community.st.com/s/question/0D50X0000AAI2pESQT/stm32h743ii-spidma-malfunction