cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 series - brutal raw power of 400MHz clock

waclawek.jan
Super User
Posted on October 20, 2016 at 11:10

While I see no announcement, the following is online:

http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32h7-series.html?querycriteria=productId=SS1951

Not only the 400MHz Fclk is worth mentioning, but also 1MB of RAM (64kB ITCM + 128kB DTCM, the rest is a 3-part user SRAM  and 4kB backup SRAM)

JW

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Amel NASRI
ST Employee
Posted on October 20, 2016 at 15:32

http://www.st.com/content/st_com/en/about/media-center/press-item.html/p3878.html

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

jpeacock23
Associate III
Posted on October 21, 2016 at 21:18

It looks like a nice fit below an A series based controller.  An M7 is a lot easier to use compared to going the A5, A7, A9 or an old ARM11 route.  Forcing that jump to SDRAM from flash and internal SRAM adds a lot to the BOM cost, plus the layout hassles going to BGA and extra PCB layers.

By coincidence just after reading about the H7 I was handed a problem that needs a custom built gateway from proprietary radio to Ethernet.  The H7 is fast enough to handle the thruput and large enough memory that I don't have to look at an A7.  Timing for the announcement could not be better....

  Jack Peacock

waclawek.jan
Super User
Posted on November 16, 2016 at 13:43

In action, http://blog.st.com/see-new-stm32h7-mcu-action/

The real stuff is from 2:15.

This of course does not demonstrate the powers of 'H7xx, but that of the built-in hardware JPEG decoder. Pretty, though.

A few pictures of the evalboard used in that demo: http://time4ee.com/articles.php?article_id=35

JW

AvaTar
Lead
Posted on November 16, 2016 at 14:14

> It looks like a nice fit below an A series based controller.  An M7 is a lot easier to use compared to going the A5, A7, A9 or an old ARM11 route.  Forcing that jump to SDRAM from flash and internal SRAM adds a lot to the BOM cost, plus the layout hassles going to BGA and extra PCB layers.

 

Depends on one's viewpoint (i.e. requirements).

A Cortex A (or another ''real'' CPU) allows a proper OS environment like Linux, with a huge quantity of available and free software, including developers.

For certain projects, hardware design costs are less of a driving factor.

With this in mind, I'm not really surprised by the rather reluctant market acceptance of M7 devices.

waclawek.jan
Super User
Posted on November 16, 2016 at 14:22

> reluctant market acceptance of M7 devices

Do you have numbers or any other fact in supporting this?

Thanks,

JW

AvaTar
Lead
Posted on November 16, 2016 at 15:37

> Do you have numbers or any other fact in supporting this?

No - just statements of MCU vendor staff at trade shows.

And, of course, project discussions at my company/companies that I witnessed.

AvaTar
Lead
Posted on November 16, 2016 at 15:45

To add another comment:

Does not speak the number of available M7 silicons (and the number of M7 licensees) speak for itself ?

But that might as well have to do with the ongoing ''consolidation process'' in the MCU world (which gives me kind of a headache ...).

AvaTar
Lead
Posted on November 23, 2016 at 13:05

Here

http://www.elektroniknet.de/design-elektronik/halbleiter/komplexe-mcus-beherrschbar-machen-134788.html

about a multi-vendor round table discussion, coming to similar conclusions. However, in German language.

waclawek.jan
Super User
Posted on November 23, 2016 at 13:55

Thanks, AvaTar.

Jan