STM32G4xx FDCAN Delay Compensation
A little something I have noticed today. I have been developing an application which is using the G431 and uses FD-CAN. My code was working in External Loopback mode such that a CAN message of my choosing was being correctly received by an external device, yet in Normal mode otherwise the same code was creating error frames.
I had used the ST-provided HAL function HAL_FDCAN_ConfigTxDelayCompensation to ensure the self-reception of the message was compensated for the 4Mb/s bit rate I have chosen for the data part of the CAN frame.
The error frames were caused because there is a bit in the FDCAN_DBTP register which controls the delay compensation method which is not set by the ST-provided HAL function. This bit may be configurable elsewhere in the GUI or by other HAL functions, but it seems to me that a function designed to configure the delay compensation should include it where a non-zero time offet is desired.
For those who do not use the HAL, the DBTP register is part of the FDCAN_GlobalTypeDef struct - TDC is bit 23 of this register and must be set to true to enable delay compensation - see G431 Reference Manual Rev 2 page 1928.
My code now works so I can start to work on the Receive Message side.
I hope this helps somebody.