Skip to main content
Tobe
Senior III
May 1, 2024
Question

STM32G431 - ADC wont get ready with 128 and 64 prescaler.

  • May 1, 2024
  • 0 replies
  • 625 views

Hi,

when investigating issues with the DMA, i found, that the prescaler is not working properly.

At 128 and 64 setting, the initialization of the ADC does not even finish. It is stuck in the loop after enabling the ADC.

 

 

	SET_BIT(RCC->AHB2ENR, RCC_AHB2ENR_ADC12EN);
	delayMicroseconds(1); 	// CAUTION: 	Just after enabling the clock for a peripheral, software must wait for a delay before accessing the peripheral registers.
	SET_BIT(RCC->CCIPR, RCC_CCIPR_ADC12SEL_1);	// PLL clock?
	//ADC12_COMMON->CCR |= (ADC_CCR_CKMODE_1 | ADC_CCR_CKMODE_0);		// adc_hclk/4

	delayMicroseconds(1);
	ADC12_COMMON->CCR |= ADC_CCR_PRESC_3 | ADC_CCR_PRESC_1 | ADC_CCR_PRESC_0;

	ADC1->CR &= ~ADC_CR_DEEPPWD;	// Disable power down (is default after reset)
	ADC1->CR |= ADC_CR_ADVREGEN;	// Enable voltage regulator

	delayMicroseconds(25); 			// Wait for voltage regulator to start up (fixed value of datasheet!)
	ADC1->CR |=	ADC_CR_ADCAL;		// Calibrate single ended (ADCALDIF is default 0)

	while(ADC1->CR & ADC_CR_ADCAL);	// Wait until calibration has finished
	delayMicroseconds(1); 			// ADC can only be enabled after short wait after ADCAL

	ADC1->ISR |= ADC_ISR_ADRDY;		// Clear ready bit by writing 1, for reading the right status below
	ADC1->CR |=	ADC_CR_ADEN;		// Enable ADC

	while((ADC1->ISR & ADC_ISR_ADRDY) == false); 					// Wait until ready

 

Is there a limitation, that i am not aware of?

This topic has been closed for replies.