2022-08-29 1:09 AM
I am getting this following error while trying to debug the Custom Board.
please help me find out what is the meaning of this error.
Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
0x1fff5a30
<signal handler called>() at 0xfffffff9
frame_dummy() at 0x80000e0
__libc_init_array() at 0x8017084
Reset_Handler() at startup_stm32g0b0retx.s:98 0x8010bb2
2022-09-06 5:40 AM
Hi @HPATH.1 ,
Could you please provide some more details about the issue you are facing: which IDE? for which example is problem faced?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-09-06 7:36 AM
I am using STM32CubeIDE Version 1.8.0
Project configured for STM32GOB0RET6
But prototype is fitted with STM32GOB1RET6.
It is custom board with Custom Application. new prototype board being testing.
I tested Timer, UART, PWM working fine. Finally I started testing ADC eight channel used.
that time, sometimes it is not executing application and stuck.
I used debug LED to switch on after reset. it is not getting on.
then I tried to debug using IDE. I got this error.
one mistake I did was using uint8_t variable adcTick as 16bit variable as adcTick in TIM6 interrupt. it was incrementing to 400
I am using same timer as interval timer and also Starting ADC conversion,
below is the code. after correcting it also it did not solve the problem.
void Timer6Tick()
{
if (HAL_ADC_Start(&hadc1) != HAL_OK)
{
Error_Handler();
}
// 40000 ticks per second devided by 400 to get 100 ticks per second
adcTick++;
if(adcTick == 400)
{
adcTick = 0;
}
else
return;
// 100 ticks per second here.
tick++;
if(tick < 10)
return;
// 10 ticks per second here.
tick = 0;
}
// Timer6 INIT
// 40000 ticks per second
HAL_StatusTypeDef MX_TIM6_Init(void)
{
RCC_ClkInitTypeDef clkconfig;
uint32_t uwTimclock = 0;
uint32_t uwPrescalerValue = 0;
uint32_t pFLatency;
/*Configure the TIM6 IRQ priority */
HAL_NVIC_SetPriority(TIM6_IRQn, 2 ,0);
/* Enable the TIM6 global Interrupt */
HAL_NVIC_EnableIRQ(TIM6_IRQn);
/* Enable TIM6 clock */
__HAL_RCC_TIM6_CLK_ENABLE();
// TIM_MasterConfigTypeDef sMasterConfig = {0};
/* Get clock configuration */
HAL_RCC_GetClockConfig(&clkconfig, &pFLatency);
/* Compute TIM6 clock */
uwTimclock = HAL_RCC_GetPCLK1Freq();
/* Compute the prescaler value to have TIM6 counter clock equal to 1MHz */
uwPrescalerValue = (uint32_t) ((uwTimclock / 1000000) - 1);
/* Initialize TIM6 */
htim6.Instance = TIM6;
/* Initialize TIMx peripheral as follow:
+ Period = [(TIM6CLK/100) - 1]. to have a (1/100) s time base.
+ Prescaler = (uwTimclock/1000000 - 1) to have a 1MHz counter clock.
+ ClockDivision = 0
+ Counter direction = Up
*/
htim6.Init.Period = (1000000 / 40000) - 1;
htim6.Init.Prescaler = uwPrescalerValue;
htim6.Init.ClockDivision = 0;
htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
if(HAL_TIM_Base_Init(&htim6) == HAL_OK)
{
/* Start the TIM time Base generation in interrupt mode */
return HAL_TIM_Base_Start_IT(&htim6);
}
/* Return function status */
return HAL_ERROR;
}.