cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G070 Internal RTC Wake Up Interrupt hangs. After few iterations rtc wake up interrupt is hangs. Help will be appreciated.

Gvenk.482
Associate

  if(low_power_mode == 1)

  {

    standby(10);

    HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);    

  }

void standby(int seconds) 

{

 /* Clear all related wakeup flags*/

  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2);

  rtc_set_wake_up_timer_s(seconds);

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON,PWR_STOPENTRY_WFI);

}

void rtc_set_wake_up_timer_s(uint32_t sec)

{

  uint32_t clock = RTC_WAKEUPCLOCK_CK_SPRE_16BITS;

  // HAL_RTCEx_SetWakeUpTimer_IT will assert that delta is 0xFFFF at max

  if (delta > 0xFFFF) {

    delta -= 0x10000;

    clock = RTC_WAKEUPCLOCK_CK_SPRE_17BITS;

  }

  hrtc.Instance = RTC;

  HAL_StatusTypeDef status = HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, delta, clock);

  if (status != HAL_OK) {

    // debug("Set wake up timer failed: %d\n", status);

    NVIC_SystemReset();

   }

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0