STM32G041C8T6 Issue with Simple ADC conversion
Hello,
I am using STM32G041C8T6 controller and I am facing an issue with ADC even for a simplest conversion on ADC Channel 0. I am providing 2.12V on the Channel 0 (PA0) pin and the conversion result is always 4095. The signal comes from a voltage divider, tapped from the mid point of two 10K resistors put between 5V and GND. Infact the resistor towards the ground is a 10K NTC temperature sensor, so at 25*C the voltage is exactly 2.5V, and decreses with increasing temperature. I'm not using any DMA, interrupts, just polling as per the reference code for G0 series.
I am following the simplest conversion of 1 channel with the following initialization from CubeIDE:
static void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.LowPowerAutoPowerOff = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_39CYCLES_5;
hadc1.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_39CYCLES_5;
hadc1.Init.OversamplingMode = DISABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}The main contains:
#define VDDA_APPLI 3300
uint16_t temp_val_adc;
uint16_t adc_converted_data[4];
/* Run the ADC calibration */
if (HAL_ADCEx_Calibration_Start(&hadc1) != HAL_OK)
{
/* Calibration Error */
while(1);
}
/* Start ADC conversion */
if (HAL_ADC_Start(&hadc1) != HAL_OK)
{
/* ADC conversion start error */
while(1);
}
/* Wait for the first ADC conversion to be completed (timeout unit: ms) */
if (HAL_ADC_PollForConversion(&hadc1, 2) != HAL_OK)
{
/* ADC conversion start error */
while(1);
}
while(1)
{
adc_converted_data[0] = HAL_ADC_GetValue(&hadc1); //adc_converted_data[0] always 4095.
/* Compute the voltage */
temp_val_adc = __LL_ADC_CALC_DATA_TO_VOLTAGE(VDDA_APPLI, adc_converted_data[0], hadc1.Init.Resolution );
HAL_Delay(500);
LED_RED_TOGGLE;
}
The APB is running on 16MHz (HCLK), SYSCLK is 64MHz. I have observed the same behavior on more than one board. Can anyone suggest what I'm missing, this code ran perfectly on F4 Disco boards, but now I'm baffled by it.
Thanks in advance for any support.
-Regards,
Munish