STM32G030 Flash Read/Write issues.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-05 2:27 AM
>>Hi I am trying to write and read data from FLASH in STM32G030 32KB Flash device.
>>However , I am experiencing unusual behavior . Sometimes I am able to read data correctly and sometimes junk data is read.
Following is my code :
#define FLASH_USER_START_ADDR 0x08007800UL
#define FLASH_USER_END_ADDR 0x08007FFFUL
uint32_t FirstPage = 0, NbOfPages = 0;
uint32_t Address = 0, PageError = 0;
static FLASH_EraseInitTypeDef EraseInitStruct = {0};
uint32_t count_f_life_data=0;
uint32_t count_one_yr_data=0;
uint32_t eep_pre_tim1_arr_prd =136;
uint32_t eep_reg_tim1_arr_prd =280;
void Write_Data_Flash2()
{
uint32_t Page_error_status;
HAL_FLASH_Unlock();
/* Clear OPTVERR bit set on virgin samples */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
FirstPage = GetPage(FLASH_USER_START_ADDR);
NbOfPages = GetPage(FLASH_USER_END_ADDR) - FirstPage + 1;
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Page = FirstPage;
EraseInitStruct.NbPages = NbOfPages;
HAL_FLASHEx_Erase(&EraseInitStruct, &Page_error_status);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x08007800UL, eep_pre_tim1_arr_prd);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x08007808UL, eep_reg_tim1_arr_prd);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x08007810UL, count_f_life_data);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, 0x08007818UL, count_one_yr_data);
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
HAL_FLASH_Lock();
}
void Read_Data_Flash2()
{
//HAL_FLASH_Unlock();
eep_pre_tim1_arr_prd = *(__IO uint32_t *)0x08007800UL;
eep_reg_tim1_arr_prd = *(__IO uint32_t *)0x08007808UL;
count_f_life_data = *(__IO uint32_t *)0x08007810UL;
count_one_yr_data = *(__IO uint32_t *)0x08007818UL;
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
//HAL_FLASH_Lock();
}
Kindly help.
- Labels:
-
Flash
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-05 5:20 AM
What exactly is "junk data" and how do they differ from good ones? Once junk, are all data junk or only some of them? Do you read/check them immediately after writing? Check after erase if the given address is blank.
Is this a "known good" hardware such as Nucleo or Disco?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-05 5:28 AM
1 . Sorry , data isn't junk .... while reading data , I see only 0xFFFFFFFF
2.I am writing to 4 locations , 3 locations return correct data , while one location return 0xFFFFFFF , it's random and not fixed for a location.
3.Yes I'm trying to read immediately after writing ....I took code help from STM32G0 example .
4.I have observed than whenever I have a read/write operation , my debugger stops responding properly.
5.We have customized board having STM32G030 IC.