cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G030 ADC issue

MFaiz.2
Associate II

Hello,

I am using STM32G030C8 microcontroller's several ADCs. Most of them are working okay but two of them (ADC1 IN15, PB11 and ADC1 IN16, PB12) are not showing correct ADC values.

In ADC IN15: When I use only this channel in the code then it shows 0 but when I read multiple channels it shows the value of the channel which is read before it.

In ADC IN16: The value is always very low regarding the actual voltage on that pin.

My VREF is 2.5V. I generated the code with CubeMX and using Keil IDE.

I have tested it in more than 1 hardware with same results. Also I have technically verified the voltage at the pin. The voltage at said pin is varied from 1.2V to 1.5V. Same type of input signals are applied to ADC channels 7,8,9,10,11 and reading values without any issues.

Also uploading the project for reference

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
waclawek.jan
Super User

Sounds like high input signal impedance/inadequate sampling time.

What's the input signal source?

JW

Input is driven by opamp. I am sure this is not an input issue because 5 other channels are connected with same type of input but they are showing correct readings.

TDK
Super User

Check your CHSELRMOD bit. If it's 1, only channels 0-14 may be selected for regular conversion.

0693W000003OwMpQAK.png

If it's 0, you can select any channel.

0693W000003OwPTQA0.png

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Super User

Set it up in CubeMX to see the correct code to convert channel 15+.

If you feel a post has answered your question, please click "Accept as Solution".
waclawek.jan
Super User

Humm, ST gets really inventive in the ADCs... no two alike... TDK, don't you happen to know, this "feature", is it present in any other STM32 family too?

JW

It’s the first time I’m seeing it. It is certainly not in the families I’ve used a lot in the past. F4, H7
I first tried to set it up in CubeMX and it reported an error, so I investigated the reference manual.
If you feel a post has answered your question, please click "Accept as Solution".

@Community member​ 

I have also used STM32F407VG's all ADC channels without such weird issue

@TDK​ 

I have used CubeMX, though it didn't give me any error. Original project files are attached with question

CHSELRMOD_bit is 0 as shown in screenshot

 As you can see, channel_15 value is exactly same as channel_3 value because it is read before channel_15.

If I disable all other channels and only enable channel_15 then it will read exact 0.

Interesting point is all HAL functions return OK status.

TDK
Super User

> I have used CubeMX, though it didn't give me any error. Original project files are attached with question

Your project only converts a single channel, channel 3. The error is not in the CubeMX generated code, it's in the user code you added.

Channels 1, 15 and 16 are set up as inputs, but they're not actually part of the conversion in your project.

0693W000003OxMBQA0.png

If you feel a post has answered your question, please click "Accept as Solution".