cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F769 Reference manual

sascha23
Associate II
Posted on May 02, 2016 at 08:50

Hi,

where can i find the reference manual of STM32F769? The STM32F7 page just contains the RM0385 which is applicable for STM32F75xxx and STM32F74xxx. Is this RM also applicable for the STM32F76xxx because it is not stated in the introduction of this document?

Thanks.
5 REPLIES 5
Walid FTITI_O
Senior II
Posted on May 02, 2016 at 11:56

Hi neumann.sascha,

STM32F769xx device is not yet generated.

Once the device is on the market, both datasheet and reference manual will be published on the web. However, you can contact you FAE if need early/ quick information.

-Hannibal-
Walid FTITI_O
Senior II
Posted on May 27, 2016 at 15:52

Hi neumann.sascha,

STM32F769xx is available now. You find relevant datasheet on the web at this

http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32f7-series/stm32f7x9/stm32f769ii.html

-Hannibal

sascha23
Associate II
Posted on June 24, 2016 at 09:56

Hi,

thank you. In the reference manual section 24 - ''Hash processor'' is written that the section only applies for the STM32F756xx but the manual is valid for the STM32F76xxx and STM32F77xxx. That might be a wrong documentation.

So applies the hash processor for the F766 and F776?

sascha23
Associate II
Posted on June 24, 2016 at 09:57

The same problem exists for the chapter 23 - Cyptographic processor

Posted on June 24, 2016 at 15:01

ST has historically had product with and without HASH/CRYPT depending on the markets they can be sold into. They are otherwise identical, and having two manuals makes no sense. Sometimes the product offering will be a subset of the possible feature set.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..