2016-05-01 11:50 PM
Hi,
where can i find the reference manual of STM32F769? The STM32F7 page just contains the RM0385 which is applicable for STM32F75xxx and STM32F74xxx. Is this RM also applicable for the STM32F76xxx because it is not stated in the introduction of this document? Thanks.2016-05-02 2:56 AM
Hi neumann.sascha,
STM32F769xx device is not yet generated.Once the device is on the market, both datasheet and reference manual will be published on the web. However, you can contact you FAE if need early/ quick information.
-Hannibal-2016-05-27 6:52 AM
Hi neumann.sascha,
STM32F769xx is available now. You find relevant datasheet on the web at this -Hannibal2016-06-24 12:56 AM
Hi,
thank you. In the reference manual section 24 - ''Hash processor'' is written that the section only applies for the STM32F756xx but the manual is valid for the STM32F76xxx and STM32F77xxx. That might be a wrong documentation. So applies the hash processor for the F766 and F776?2016-06-24 12:57 AM
The same problem exists for the chapter 23 - Cyptographic processor
2016-06-24 6:01 AM
ST has historically had product with and without HASH/CRYPT depending on the markets they can be sold into. They are otherwise identical, and having two manuals makes no sense. Sometimes the product offering will be a subset of the possible feature set.