Skip to main content
Pilous Droip
Senior
May 30, 2018
Question

STM32F767 and SPI communication without DMA

  • May 30, 2018
  • 20 replies
  • 2632 views
Posted on May 30, 2018 at 08:34

Hello friends,

I try SPI communication, and I have a problem. I only send data.... But how to receive it?

Connection is:

1. one master - one slave

2. Full duplex

Initialize:

LL_SPI_InitTypeDef SPI_InitStruct;

LL_GPIO_InitTypeDef GPIO_InitStruct;

LL_SPI_Disable(SPI1);

LL_AHB1_GRP1_EnableClockLL_AHB1_GRP1_PERIPH_GPIOA);

LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);

/* SPI2 GPIO Configuration */

GPIO_InitStruct.Pin = LL_GPIO_PIN_5;

GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;

GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;

GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;

GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIO_InitStruct.Pin = LL_GPIO_PIN_7;

GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;

GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;

GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;

GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIO_InitStruct.Pin = LL_GPIO_PIN_6;

GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;

GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;

GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;

GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIO_InitStruct.Pin = LL_GPIO_PIN_4;

GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;

GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;

GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;

GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;

GPIO_InitStruct.Alternate = LL_GPIO_AF_5;

LL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/* SPI1 parameter configuration*/

SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;

SPI_InitStruct.Mode = LL_SPI_MODE_MASTER;

SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;

SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_HIGH;

SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;

SPI_InitStruct.NSS = LL_SPI_NSS_HARD_OUTPUT;

SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV64;

SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;

SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;

SPI_InitStruct.CRCPoly = 7;

LL_SPI_Init(SPI1, &SPI_InitStruct);

LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);

LL_SPI_EnableNSSPulseMgt(SPI1);

LL_SPI_SetRxFIFOThreshold(SPI1, LL_SPI_RX_FIFO_TH_QUARTER);

/* Configure SPI1 transfer interrupts */

/* Enable RXNE Interrupt */

LL_SPI_EnableIT_RXNE(SPI1);

LL_SPI_Enable(SPI1);

And function to write/read....

int32_t read_from_reg(SPI_TypeDef *SPI, uint8_t data, uint8_t *SPI_Data_receive)

{

LL_SPI_TransmitData8(SPI, data);

while (!LL_SPI_IsActiveFlag_TXE(SPI));

while (!LL_SPI_IsActiveFlag_RXNE(SPI));

while (LL_SPI_IsActiveFlag_BSY(SPI));

*SPI_Data_receive = LL_SPI_ReceiveData8(SPI);

return 0;

}

And I sent one byte and I don't receive anything. Any idea, how to receive some data from register?

#nucleo-f767zi #stm32f7-spi

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This topic has been closed for replies.

20 replies

T J
Senior III
May 30, 2018
Posted on May 30, 2018 at 09:21

I don't use the LL chips, but my running code runs along these lines.

int32_t read_from_reg(SPI_TypeDef *SPI, uint8_t data, uint8_t *SPI_Data_receive)

{

   LL_SPI_TransmitData8(SPI, data);            // issue 8 clocks to send command

   while (!LL_SPI_IsActiveFlag_TXE(SPI));   // wait while not empty

   while (LL_SPI_IsActiveFlag_BSY(SPI));   // wait while busy,

   //now byte has been clocked out

  while (!LL_SPI_IsActiveFlag_RXNE(SPI))  // you should read & dump all bytes in the Rxregister now

      read SPI_DR;

*SPI_Data_receive = LL_SPI_ReceiveData8(SPI);  // issue new 8 clocks to read data

   return 0;

}
Pilous Droip
Senior
May 30, 2018
Posted on May 30, 2018 at 09:44

I modificated it, and no change ......

How it have to have look:

And here is how it look now:

read_from_reg(SPI1, 0xF0, read);

0690X0000060BQFQA2.png

T J
Senior III
May 30, 2018
Posted on May 30, 2018 at 10:33

you only show 8 clock cycles..

What instruction is it ? 8 bit ?

that has to be transmitted,

then you want to receive 8 bits ?

you must transmit again, to receive those 8 bits.

Pilous Droip
Senior
May 30, 2018
Posted on May 30, 2018 at 11:52

I try everything. 

>:(

For example, when I send 0xAB so chip must return his ID in 24bits.

So I send 0xAB and receive nothing. And clock doesn't generate signal. 

0690X0000060L12QAE.png

And yes, I can resend instruction, but is this solution good?

stm322399
Senior
May 30, 2018
Posted on May 30, 2018 at 11:59

If I am right, NSS pulsed mode will drive CE high between byte, and this is not what your target device expects. Try without.

Recently I ran with HW NSS correctly by pulling-up the NSS pin, I suspect that its drived by SPI as ope drain.

Good luck.

Pilous Droip
Senior
May 30, 2018
Posted on May 30, 2018 at 12:42

 ,

 ,

I modificated NSSPulse to disable, and now SPI is dead.

Actual settings:

SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX,

 ,

SPI_InitStruct.Mode = LL_SPI_MODE_MASTER,

 ,

SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT,

 ,

SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_HIGH,

 ,

SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE,

 ,

SPI_InitStruct.NSS = LL_SPI_NSS_HARD_OUTPUT,

 ,

SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV128,

 ,

SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST,

 ,

SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE,

 ,

SPI_InitStruct.CRCPoly = 7,

 ,

LL_SPI_Init(SPI, &,SPI_InitStruct),

LL_SPI_SetStandard(LL_SPI_PROTOCOL_MOTOROLA),

 ,

LL_SPI_DisableNSSPulseMgt(SPI),

LL_SPI_SetRxFIFOThreshold(SPI, LL_SPI_RX_FIFO_TH_QUARTER),

LL_SPI_Enable(SPI),

Read FCNT

void TM_SPI_Read(SPI_TypeDef* SPIx, uint8_t* dataIn, uint8_t dummy, uint8_t count)

 ,

{

 ,

/* Check if SPI is enabled */

 ,

SPI_CHECK_ENABLED(SPIx),

/* Wait for previous transmissions to complete if DMA TX enabled for SPI */

 ,

SPI_WAIT_TX(SPIx),

while (count--) {

 ,

/* Wait busy */

 ,

SPI_WAIT_TX(SPIx),

/* Fill output buffer with data */

 ,

SPIx->,DR = dummy,

/* Wait for SPI to end everything */

 ,

SPI_WAIT_RX(SPIx),

/* Save data to buffer */

 ,

*dataIn++ = SPIx->,DR,

 ,

}

 ,

}

other definitions:

♯ define SPI_CHECK_ENABLED(SPIx) ,  ,  ,  ,  ,  ,  ,if (!((SPIx)->,CR1 &, SPI_CR1_SPE)) {return,}

♯ define SPI_WAIT_TX(SPIx) while ((SPIx->,SR &, SPI_SR_TXE) == 0 || (SPIx->,SR &, SPI_SR_BSY))

 ,

♯ define SPI_WAIT_RX(SPIx) while ((SPIx->,SR &, SPI_SR_RXNE) == 0 || (SPIx->,SR &, SPI_SR_BSY))
Jan Waclawek
Visitor II
May 30, 2018
Posted on May 30, 2018 at 12:50

Read out and check/post the SPI registers content.

JW

waclawek.jan
Super User
May 31, 2018
Posted on May 31, 2018 at 13:00

If the same simple program works when PA15 is used as NSS, but not if PA4 is used as NSS, then it's time to talk to ST's support...

JW

Pilous Droip
Senior
May 31, 2018
Posted on May 31, 2018 at 15:16

I reconnected it back to PA4 and it's working.

Because my first test function was without LL_SPI_Enable/LL_SPI_Disable.
Linas L
Senior
August 12, 2018

Hey. If it has 4 words fifo, how can i send only one or two data packets ? :(