cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F74NG Discovery SWO external debug

GBurn
Associate

I broke the USB connector on my disco board so can't flash it. Does anyone have experience using an external ST-Link debugger via the CN8 connector?

1 REPLY 1

STM32746G-DISCO?

CN8 is going to be entirely useless, it is there to program the STM32F103 of the ST-LINK

Where you need to get connectivity is the target side of SB14, SB15, SB16 and SB17, and removing the 0-ohm resistors.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..