cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G DISCOVERY LwIP example doesn't work. Why?

serefatakan
Associate II

 Hello world. This is my first question in here.

I am using STM32F746G DISCOVERY board and willing to know how LwIP work. But in Cube_FW_F7 LwIP example (in Applications folder) it returns a "No such a file or directory" error. Can't find deprecated_definitions.h first. I entered the path to directories and now it can't find portmacro.h.

I have tried to enter path, switching architecture (CM7 to CM4F or CM7_MPU), copy headers to project directly, but no success. I thought it would be built when I debug it.

Edit: using Atollic TrueSTUDIO 9.2.0

Edit 2: Directory problem has been solved, but it stalled in function: vPortRaiseBASEPRI() in portmacro.h

0 REPLIES 0