2017-01-16 09:53 AM
I bought a STM32F746G-DISCO board and have decided that a board like it will fit the needs of my project. Are there any companies that make development boards with this MCU that can use a larger LCD display? The disco board has a 40 pin RGB interface with the touch pins combined within the 40 pins and I can't seem to find a larger LCD panel that has this connector. Do any companies make other boards for this MCU?
#stm32f7 Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-05-30 02:21 PM
This is How we solved the issue of having a small 4.3'' and also non sunlight readable LCD.