cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO display panel choice and alternatives

ray23
Associate II
Posted on January 16, 2017 at 18:53

I bought a STM32F746G-DISCO board and have decided that a board like it will fit the needs of my project. Are there any companies that make development boards with this MCU that can use a larger LCD display? The disco board has a 40 pin RGB interface with the touch pins combined within the 40 pins and I can't seem to find a larger LCD panel that has this connector. Do any companies make other boards for this MCU?

#stm32f7

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This discussion is locked. Please start a new topic to ask your question.
30 REPLIES 30
LMI2
Lead
Posted on January 19, 2017 at 16:56

Somewhere in the 746 Discovery documents was the name of display manufacturer. Contact them, I did and got a good anwser..

I cant find the name now here.

Posted on January 19, 2017 at 17:39

https://www.alibaba.com/trade/search?fsb=y&IndexArea=product_en&CatId=&SearchText=STM32F746G+

is your friend. Low cost, good delivery times and generally high quality.
Posted on January 19, 2017 at 17:19

ROCKTECH

FPU330ZH-BT1D3-CA

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 19, 2017 at 17:43

https://community.st.com/0D50X00009XkduYSAR

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ray23
Associate II
Posted on January 19, 2017 at 18:00

I have tried to contact them, they don't even list this display on their product page.  When I tried I got no response.  Is it possible you can find your response so I can send to other then the web page address?

Posted on January 19, 2017 at 18:12

 ,

 ,

Thank you for your response.

♯ 3 is definitely beyond my capability. I am a software guy, and need a hardware plug and play solution, unfortunately.

♯ 2 seems interesting, I will look for these devices.  ,Do you have a reference to any?

♯ 1 I have looked into this, I have even thought of building an adapter that uses separate ,touch pin and integrates them to match the 746g connector.  ,Since I can't build this myself, and I can't find one I have to find a different solution.

Posted on January 19, 2017 at 18:39

Alibaba is good for higher quantity orders. If your minimum order is one or dozen pieces then Aliexpress might be a better choice. If an item is listed, price is listed and you can buy immediately.

Posted on January 19, 2017 at 18:50

nefarious wrote:

♯ 2 seems interesting, I will look for these devices.  Do you have a reference to any?

32F769IDISCOVERY is

http://www.st.com/en/evaluation-tools/32f769idiscovery.html

.

B-LCDAD-HDMI1 (MIPI-DSI to HDMI) is

http://www.st.com/en/development-tools/b-lcdad-hdmi1.html

.

I'm quite sure that you can buy these at DigiKey, Mouser, Farnell, etc.

As for the panel driver boards, just open Aliexpress.com web page and search for the numbers.

For example, if you search for number

32344321657 

it will open

https://www.aliexpress.com/item/10-1-Inch-40pins-1280-RGB-800-TFT-EJ101IA-01G-LCD-Screen-Display-With-Remote-Driver/32344321657.html

link.
Posted on January 19, 2017 at 18:57

Yes definitely at DigiKey and Mouser, run about $30 USD

The connector is the same as the one on the Arduino OTTO STAR.

I'd like to see a board with a VGA/DVI connector, got plenty of cheap monitors. Would take a F7/H7 DISCO board with an HDMI

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 19, 2017 at 19:12

We buy one, two and sometimes four units at a time. We contact the manufacturers directly and you can too. We purchase lots of stuff from China. Alibaba and Aliexpress and taobaofocus, they're all giant online catalogs, but you don't have to buy through them, you get better service by establishing a relationship directly with the manufacturer.