2018-03-07 9:06 PM
I am using STM32F746G Discovery board . I am facing an issue with image size.
My binary size is more than 1MB and gets an errorc:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.15.0.201708311556/tools/compiler/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/ld.exe: STM32F746emWin.elf section `.rodata’ will not fit in region `FLASH’c:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.15.0.201708311556/tools/compiler/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/ld.exe: region `FLASH’ overflowed by 106964 bytescollect2.exe: error: ld returned 1 exit statusmakefile:43: recipe for target ‘STM32F746emWin_ATMEGD10.elf’ failedmake: *** STM32F746emWin.elf Error 1How can I keep my image in external flash and execute from there
Can I use internal and external flash together continuesly .How can I do this ? Can any body help me to do it
2018-03-08 1:38 AM
You cannot flash more than one 1 MiB in a chips that has only 1 MiB Flash. There are two things to consider:
- Why is the image that big?
- Ths STM32F746G has the same die as a STM32F746I. Either the flash above 1 MiB is switched of with some fuse, not tested or tested bad. Try to link for STM32F746I, flash and compare the result. Perhaps you have luck.
2018-03-08 2:49 AM
Thank you.
Image became big that i am using more bmp images in code .
So it increases to more than 1MB
So I am trying to put binary in External Flash of STM32F746Discovery board
Discovery board has 128-Mbit Quad-SPI Flash memory
128-Mbit SDRAM (64 Mbits accessible).But I don't have idea to work in external Flash
2018-03-08 3:32 AM
So use the right section indicator in your code to put the BMP file into QSPI. Do not forget to initialize QSPI in your code.
2018-03-08 3:44 AM
Thanks You.
I did n't get much clarity on your comment. '
right section indicator in your code
' . I didn't get this meaning.
Actually I am using ST em Win Library for GUI development . So my BMP file convert to c code using utility (BmpCvtST)
and integrate with application using ST em win library.Then my whole binary size get increased and crossed more than 1 MB.
So I planned to keep the Binary in external flash (NOR flash) and start Run from there.
But I dont have much idea on it .
Do you have any supporting / Reference link or document to do this.
2018-03-08 5:07 AM
What about asking google about 'gcc section' ?