cancel
Showing results for 
Search instead for 
Did you mean: 

I am currently working with the STM32F746G-Disco development board and a 7-inch capacitive touch LCD. The size of the generated hex file exceeds the capacity of the internal flash memory. As a solution, I have added an external flash memory (N25Q128A).

Gc.2
Associate

Could you please provide guidance on how to flash the firmware and configure the system to boot from the external memory? Thank you!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0