2018-04-18 7:34 AM
Hi,
in the moment i build my own STM32F746 Board that is based on the STM32F746DISCO.
So i found an error in the BSP-File 'stm32746g_discovery_lcd.c'.
I use a new LCD Display with touch (other than on DISCO) and changed the SDRAM to 32-Bit databus. So i must change some processorpins!
In STM32F746DISCO the pin PI13 is named 'LCD_INT'. This is the signal 'TS_INT_PIN' in the CUBE software. This is the interrupt output of the touchscreen controller! But this interrupt function of the touchscreen is not used in the CUBE examples!
Now in the function '__weak void BSP_LCD_MspInit(LTDC_HandleTypeDef *hltdc, void *Params)' there is this pin programmed as (see bold text):
gpio_init_structure.Pin = GPIO_PIN_9 | GPIO_PIN_10 | \
GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15; // Here PIN_13 is wrong! gpio_init_structure.Mode = GPIO_MODE_AF_PP; gpio_init_structure.Alternate = GPIO_AF14_LTDC; HAL_GPIO_Init(GPIOI, &gpio_init_structure);With this PIN_13 assignment as AF14 the processor outputs the signal 'LCD_VSYNC' at PI13 and this output is connected to the interrupt output of the touch controller!
i measured at this pin the signal 'LCD_VSYNC' with a scope!!!! So we have 2 outputs connected together => we have a collision!!I removed PIN13 from the code and no more collision!
Best regards
Werner
2018-07-13 8:43 AM
Hi
Neuschwander.H.W
,Even with delay, please note that the problem you reported isn&39t lost.
So thanks for highlighting the issue, it is reported to our development team in order to be fixed in coming versions of the BSP driver for STM32746G-Discovery board.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.