2024-01-28 6:19 AM - last edited on 2024-01-30 1:04 AM by mƎALLEm
Hi,
Could anyone help with this problem? Its driving me mad!!!
I have designed an ethernet interface for an F746-100 MCU
I have changed pins to avoid using Port G and I have used the circuit below.
The RJ45 connector is a standard RB1-125BAG1A and the ethernet chip is a LAN8742A
Can anyone tell me if there are any mistakes in this?
I cannot get any connection at all - F746-100 will not ping.
Green LED ON and Yellow LED flashes continuously.
I have an STM32F746 - 144 Nucleo with the same software (apart from the two pins that are changed) -works fine.
The 25MHz xtal works OK (same signal on both boards) and the LAN8742_STATUS_OK returns 0 on both boards when I debug.
There appears to be no errors in the setup LAN8742.c or the ethernetif.c when I debug. This code works OK on the NUCLEO board and I can display a small webpage. Both sets of code use only ETH and LWIP, fixed IP, on a standard Cubeide setup. I assume that the only difference is the two GPIO allocations (PG13>PB12 and PG11>PB11) which I have altered in software.
I have the same sort of signals on both boards on TXP/TXN/RXP/RXN
Can some kind soul tell me if there is anything obviously wrong with my hardware?
Thanks.
Chris
Solved! Go to Solution.
2024-07-19 7:24 AM
Hello clock.1166,
I have a problem with custom design LAN8742 ic circuit. What is the problem for that there is no signal on the TXD0/TXD1/TXEN pins? There are signals on RXD0/RXD1 and RXN-P, TXN-P pins by the way.
2024-07-20 12:58 AM
Hi - The circuit that I posted works perfectly.
My problem was that the 49.9ohm resistors were incorrect values. After I had changed these - all was OK.
Chris