STM32F7 SAI SPDIF TX channel status / frame count
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-14 9:25 AM
Dear STM32-SPDIF-TX experts,
I'm working with a STM32F767 on a Nucleo-144 board.
Creating a sine, sending data at 24bit/192kHz via DMA / SAI 2B, everything fine.
Filling the output buffer for SPDIF within the HAL_SAI_TxHalfCpltCallback() & HAL_SAI_TxCpltCallback() functions. Works like a charm.
Now the problem:
I need to add SPDIF channel status data, that actually works too, but with one problem:
the frame count seems to be delayed by 22 bytes.
For testing I send only incremented values 1..24 (left channel, right channel + 0xA0), but what I get on the receiver side always starts like that:
22 23 24 1 2 ...
The frame counter is always reset to 0 before HAL_SAI_Transmit_DMA(), incremented in the ISRs, and reset to 0 when it reaches 192.
All the bytes I receive are okay, it's just the order of the bytes.
I do not want a "workaround", I'd like to know what I am doing wrong, or maybe if there is a problem with the DMA / SPDIF TX combination.
So, any ideas?
Thanks in advance!
- Labels:
-
DMA
-
SAI
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-14 9:36 AM
Okay, just found out that this frame count "delay" depends on the DMA buffer size:
when I set the frame counter to half DMA buffer size before starting, then the channel status data order is okay.
And I guess my problem with DMA-TX is, that I need to fill the TX buffer before starting DMA TX... ouch!
(I'm mostly working on the "receiving side" ;) )