cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 HAL Drivers for internal SRAM Access

Nandish Jasani
Associate II
Posted on February 23, 2018 at 17:39

Hello Everyone,

    I am using 32F746GDISCOVERY. My code is stored in flash memory (0x08000000) on AXIM Bus with I and D cache enabled. I am using SW4STM32 Eclipse based IDE, i used STM32Cube for configuration this MCU. Now i want access internal SRAM without DMA (Read/Write Operation). I want to write some data in internal SRAM. Is there any HAL Driver to access internal SRAM? 

    Please help for above query.

    Thanks,

Nandish Jasani.

1 REPLY 1
Posted on February 23, 2018 at 17:55

No, I think the processor just handles things. Use memcpy() or pointers...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..