2015-10-30 12:15 PM
Hello, can someone please tell me how to add succesfully BSP drivers after generating a project on Keil with STM32CUBEMX.
Thanks.2015-11-02 01:17 AM
Hi noto,
“how to add succesfully BSP drivers after generating a project on Keil with STM32CUBEMX�BSP drivers are integrated manually in the project, I don’t know which kind of problem you are facing when adding drivers.I propose that you have a look to the BSP example under STM32Cube F7 package and try to compare the project settings (include Paths, Define) with yours as first step.STM32Cube_FW_F7_V1.2.0\Projects\STM32746G-Discovery\Examples\BSP\MDK-ARM-Syrine-