2018-06-16 4:49 AM
Dear All,
I am working on STM32F4Doscovery board timers. I want to make a timer interrupt for an application. It can be 1sec or 500ms interrupt. I have read the datasheet and written the program accordingly. But i dont know how to use interrupt in STM32. I have tried something, but nothing is happening. Can someone suggest me a solution??
&sharpinclude 'stm32f4xx.h'
// Component selectionvoid GPIO_Init(void);
void tim10_init(void);
int main(void)
{ GPIO_Init(); tim10_init(); while (1) { GPIOD->ODR|=(1<<15);}
}
void GPIO_Init(void)
{ RCC->AHB1ENR|=RCC_AHB1ENR_GPIODEN; GPIOD->MODER|=(1<<28); // pin 14 is output GPIOD->OTYPER&=~(1<<14);//pin 14 as push pull GPIOD->OSPEEDR|=(1<<29)|(1<<28);//LOW speed GPIOD->PUPDR&=~(1<<29)|(1<<28);//No push pull GPIOD->MODER|=(1<<30); // pin 15 is output GPIOD->OTYPER&=~(1<<15);//pin 15 as push pull GPIOD->OSPEEDR|=(1<<30)|(1<<31);//LOW speed GPIOD->PUPDR&=~(1<<30)|(1<<31);//No push pull }void tim10_init(void)
{ RCC->APB2ENR|=(1<<17); TIM10->CR1|=(1<<7); TIM10->DIER|=(1<<1); TIM10->SR|=(1<<1); TIM10->EGR|=(1<<1); TIM10->CCMR1|=(1<<3)|(0<<1)|(0<<0); TIM10->CCER|=(1<<0); //TIM10->CCR1=5; TIM10->PSC|=4200; TIM10->ARR|=1000; NVIC_EnableIRQ(TIM1_UP_TIM10_IRQn);}void TIM10_IRQHandler(void){ GPIOD->ODR|=(1<<14); }#stm32f4-d #learning-stm32Solved! Go to Solution.
2018-06-24 2:10 PM
Here,s my stuff. Search for '
void
init_usart1
(void
)' on. It's bare metal code for STM32F103 without any libraries.https://github.com/turboscrew/blue_pill_init/blob/master/FirstTry.c
My USART-code uses interrupts and ring buffers. Select the TXE. With TC there are 'glitches'.
// use TXE as transmit interrupt instead of TC
#
define
DEBUG_UART1_TXE
2018-08-10 6:51 AM
Dear All,
NowI have been stuck with the sd card interface for last 3 weeks. I have used cubemx version 4.26 for creating this project. But F_mount function is not working.Please find the below code. I have tried everything based on youtube videos but nothing working out. kindly help me out to solve this issue.
#include "main.h"
#include "stm32f4xx_hal.h"
#include "fatfs.h"
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
SD_HandleTypeDef hsd;
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
sta
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_SDIO_SD_Init();
MX_FATFS_Init();
UINT testbyte;
HAL_Delay(10);
if(f_mount(&SDFatFS,SDPath,1)==FR_OK)
{
HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_12);
char mypath[]="WRITE1.TXT\0";
f_open(&SDFile,mypath,FA_WRITE|FA_CREATE_ALWAYS);
char *mydata="HELLO WORLD\0";
f_write(&SDFile,&mydata,sizeof(mydata),&testbyte);
f_close(&SDFile);
HAL_Delay(1000);
HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_13);
}
while (1)
{
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 50;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV4;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/* SDIO init function */
static void MX_SDIO_SD_Init(void)
{
hsd.Instance = SDIO;
hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
hsd.Init.ClockDiv = 0;
}
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13, GPIO_PIN_RESET);
/*Configure GPIO pins : PD12 PD13 */
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
}
void _Error_Handler(char *file, int line)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
while(1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */