2014-01-28 12:37 PM
I'm running the MEMs example from
STM32F4-Discovery_FW_V1.1.0\Project\Peripheral_Examples\MEMSusing uVision / MDK-ARM and I'm not getting any changing values when the read function is being called on the SysTick interrupt. I am waving it around and tapping on it but not getting anything.LIS302DL_Read(Buffer, LIS302DL_OUT_X_ADDR, 6);printf(''values : %d %d\n'', Buffer[0], Buffer[2]);values : 171 1980xAB, 0xC6These are the values that come through all the time. I've stepped into LIS302DL_Initand LIS302DL_LowLevel_Initbut there's not conditional or information on how to see if it's failed. I have two of these board so I also tested on another board and it's the same. I think when I first got the board this was the application running on it so I don't think there is a hardware issue. Thanks,Jim. #stm32f4discovery-mems2014-03-13 4:30 AM
Hi Jim,
I've tested this application available under: STM32F4-Discovery_FW_V1.1.0\Project\Peripheral_Examples\MEMS the discribed issue is not detected. Just follow the following steps: View menu - Watch Windows - Watch 1 View menu - Periodic Window Update (Should be enabled) and try to view the Buffer[] variable content (see attached file) Values are changing when moving the board embedding the MEMSaccelerometer. With regards, MPTun ________________ Attachments : KEIL_Live_Watch.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0gt&d=%2Fa%2F0X0000000bck%2F4CvIJlgSAEl0vJQA4UPTd9QLociPNwPw1bbj8ImVfPQ&asPdf=false2014-03-13 5:14 AM
!me
2014-03-13 5:55 AM
Clive2 & Jim,
I assume you are using different boards' revisions. There should be an issue when using revC (wrong driver used in the library). This issue was fixed in the STM32CubeF4 within the STM32F4-Discovery demonstration. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-03-13 7:13 AM
Jim,
Are using the STM32F4-Discovery RevC board ??The RevC does not embedd the LIS302DL MEMS accelerometer :\