2016-03-23 08:48 PM
Hi I had a couple of questions.
I'm from the software side of things and hardware is new to me!I am starting a project where I'd like to drive around 5 colour lcd's.It's a bit tricky in that I'd ideally like a mobile app to push an image to each of the lcds via HTTP and then have those images stored and able to be displayed on the lcds.I was wondering hardware wise what I'd need to investigate to make this happen and if anyone had done anything similar in the past?I'll also be driving some servos as well.Would this kind of board: STM32F4DISCOVERY be suitable? I'll need to get the wifi expansion as well.Thanks,Tom