2012-04-16 4:18 AM
Hello,
I just bought an STM32F4 discovery board. I installed the USB drivers (ST-LINK/V2 USB driver for Windows 7, Vista and XP
) and theSTM32 ST-LINK utility programmer. As a first step I would like to connect the ST-Link v2 to the device and then load an example binary file.
The programmer do not reconize the device. When trying to connect, the green/red led is blinking, and them goes to green. But the programmer give me the following message: ''21:57:55 : Connected via SWD.
21:57:55 : Cannot connect to the MCU device!
'' I tried to do a firmware update. When the board has just been connected i'm able to see the firmware version, it is up to date (i'm also able to update it). But if i try to connect the device, then after firmware update is not possible any more until rebooting the board. I think i have à driver problem. I tried everything i found on the web (like removing daemon tool) and also tried to instal the drivers on an other computer. I do not manage to connect to the device !!! Can someone may confirm that i can use the''STM32 ST-LINK utility programmer'' by itself as a very first step (to check connectivity)?
Does someone know what may I do to connect this device? I use windows 7, on a core i3 (64bits) based computer. Regards, Ronan2012-04-25 10:16 AM
Thanks, this is well working now with the patch... :)
Regards, Ronan