cancel
Showing results for 
Search instead for 
Did you mean: 

Touch configuring in microxplorer

raig
Associate
Posted on April 17, 2012 at 11:18

If I try to configure the TS module on a STM32L151 all TS pin will appear green and blocked for other use. I like to configure only 4 pins for touch. This seems to be not possible with this tool or is there a trick?

Raig

#stm32l-touch-microxplore
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Thierry GUILHOT
ST Employee
Posted on April 25, 2012 at 21:20

Hello,

I confirm you that the tool MicroXplorer is not suitable to check a configuration involving some touch sensing pins. Selecting the TS function automatically enables all the TS pins. This behavior is not correct and the tool will be updated to offer more flexibility.

Best Regards,

Thierry,