cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F479ZI CAN2 SLAVE BAUD RATE SPEED LIMIT ?

hello. i can see 500K Bps on CAN1 and i can't see this baud rate on CAN2. I use same bit timing and i can't see this baud rate. What is the maximum baud rate limit on CAN2? I attached source folders. I am waiting answer as soon as possible. Best regards.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

The clock comes from the same APB source, the prescaler and quanta settings control the wire speed.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I do not understand. Can you explain in more detail