2017-07-15 3:01 AM
I have recently got a STM32F469I-DISCOVERY board to start embedded development on STM32 family. To begin, I have downloaded the STM32F4 firmware package and started to test some of the demo applications provided. It seems that there is a graphics issue with some of these applications, specifically when loading images from the memory.
To give you some context, when I run the demo, the ST-Life Augmented logo as well as the menu items are drawn distorted (1-DemoScreen.png). When I run an application like LCD_DSI_ImagesSlider, the result is even worse with all buggy, blue-green images (2-ImageSlider.png). What do you think might be causing this, and how can I solve this?
Things I have tried/thought so far:
1) The LCD display is connected via CN10 connector. The connection seems intact and the display works totally fine.
2) In fact, I wrote a test application to test the screen colors, by drawing different colored circles all over. (3-GraphicTest.png) It seems that it can display all colors properly.
3) The loaded images seem to be stored in .h files in binary form (eg. uint32_t array of [384000] points). My current guess is that the memory address these images are aligned to, or how they are interpreted/read, is not right. This might be due to something happened to the the MCU, or a misconfiguration due to my IDE/toolchain settings.
4) As a side note, I am using SW4STM32 out of the box. I have updated the firmware of my device, however this have not solved anything.
Any ideas?
Thanks in advance,
-YiÄŸit
2017-09-12 7:03 AM
Hi - I have the exact same issue. Pre-loaded (out of the box), the graphics looked fine - but then when I actually built the demo application and loaded it on to the Discovery board, I ran into this issue. Were you able to trace the root of the problem?
Thanks.
2017-09-12 9:13 AM
>>Were you able to trace the root of the problem?
You need to load contemporaneous image data into the QSPI FLASH using the External Loader
2017-09-12 9:27 AM
2017-09-12 9:44 AM
Hi both,
Thanks for the message. Just wondered if you could help me with this error? Thanks.
2017-09-12 10:05 AM
Hi all,
How odd - the ST-LINK doesn't like it when I program via External Loader -> .. -> Program but using the Program/Verify button on the toolbar works!
Thanks,
Meenal