Skip to main content
friendlynatureperson
Associate II
April 10, 2022
Question

STM32F746 Discovery show white screen after loading F746_DISCO_FLASH.BIN using st link also emwin demo not showing any graphics after loading hex file show white screen only led blink works is TFT damaged

  • April 10, 2022
  • 6 replies
  • 1543 views

..

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
April 10, 2022

Did it work previously? As delivered?

Work directly with the vendor from whom you purchased it.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
friendlynatureperson
Associate II
April 12, 2022

Yes i membered it worked but now ONLY LCD ON WHITE SCREEN

Tesla DeLorean
Guru
April 14, 2022

Build one of the example in the CubeF7 trees for the board that uses the screen.

One of at least half a dozen, to check screen

STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Applications\Display\LTDC_PicturesFromSDCard

If the screen worked and you broke it, that's between you and the vendor.

What board revision? Is board blue or green?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Technical Moderator
April 14, 2022

Hi @friendlynatureperson​ ,

Please refer to the readme file that you find in the same folder as Binaries under Cube package. It provides the steps to follow in order to program the demonstration.

You can use either ST-Link Utility or STM32CubeProgrammer.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
friendlynatureperson
Associate II
April 15, 2022

THANKS FOR REPLY I will try examples board is green there is no scratch on LCD NOT BROKEN

friendlynatureperson
Associate II
April 16, 2022

Not working and i have to replace the tft any ideas which tft model i have to use