cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446RE: why ADC output has and offset by 300 mV for various analog input?

d146
Associate

Hi,

I'm working on STM nucleo board (STM32F446RE) currently.I'm using ADC Channel 0 and 1.I have found that the ADC output has and offset by 300 mV for various analog input. Please explain the cause.

/* code snippet to read ADC Channel 1 output*/

for( int i=0; i<SIZE; i++)

adc2[i] = TM_ADC_Read(ADC1, ADC_Channel_1);

2 REPLIES 2

How do you calculate the voltage from ADC readout? What is the input source, is it low impedance enough/is the sampling time long enough?

JW

Ozone
Lead II

ADCs are inputs.

Most probably, this offset exist already at the inputs, from your hardware.

Or, as Jan suggested, your sampling time is much too short.