2017-03-09 7:59 AM
I am using a single channel on ADC1, and a single channel on ADC2, both using DMA. Everything code-wise is working, but the ADCs appear to be fighting/resisting the inputs. For instance, with nothing connected, each ADC pin floats at ~1V. But then when you try to ground either input through a 10K resistor, I get a ~250mV triangle wave at 1MHz. Image is attached below, along with CUBE generated ADC initialization code. Any ideas on what could be causing that? I would think that grounding an ADC input through a 10K would cause the input to go to zero.
[code]
static void MX_ADC1_Init(void)
{ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV6; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.ScanConvMode = ENABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 1; hadc1.Init.DMAContinuousRequests = ENABLE; hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; //sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); }}
/* ADC2 init function */
static void MX_ADC2_Init(void){ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc2.Instance = ADC2; hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV6; hadc2.Init.Resolution = ADC_RESOLUTION_12B; hadc2.Init.ScanConvMode = ENABLE; hadc2.Init.ContinuousConvMode = ENABLE; hadc2.Init.DiscontinuousConvMode = DISABLE; hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc2.Init.NbrOfConversion = 1; hadc2.Init.DMAContinuousRequests = ENABLE; hadc2.Init.EOCSelection = ADC_EOC_SEQ_CONV; if (HAL_ADC_Init(&hadc2) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_1; sConfig.Rank = 1; //sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK) { Error_Handler(); }}
[/code]
Solved! Go to Solution.
2017-03-09 8:59 AM
If looking at a single channel per ADC, why use scan mode?
hadc1.Init.ScanConvMode = ENABLE;
What happens if the sample and hold time is increased? (because the input impedence is not low)
Otherwise, for testing pull-up/down, the internal GPIO ones can be used instead of an external physical one?
Are VDDA/VSSA well connected to board common ground/supply?
2017-03-09 8:59 AM
If looking at a single channel per ADC, why use scan mode?
hadc1.Init.ScanConvMode = ENABLE;
What happens if the sample and hold time is increased? (because the input impedence is not low)
Otherwise, for testing pull-up/down, the internal GPIO ones can be used instead of an external physical one?
Are VDDA/VSSA well connected to board common ground/supply?
2017-03-09 11:20 AM
YOU...are awesome. I had been using scan mode initially, and that was left enabled. I switched it to DISABLE, and all is well. Thanks for the help!