cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F437VIT6 Dev board recommendation

mrblueblue
Associate II
Posted on July 25, 2016 at 18:12

Hello everyone.

1.) We are going to be using the STM32F437VIT6 in a new design and would like to get going with some firmware development.  

Is there a development / demo board that you guys could recommend that has the STM32F437VIT6 on it that would be compatible with the ST-LINK/V2?

2.) For some bastic I2C, SPI and toggling pins do you think the Atollic IDE would be a good option?

Thanks.

-Mike

2 REPLIES 2
Walid FTITI_O
Senior II
mrblueblue
Associate II
Posted on July 28, 2016 at 05:28

The STM32F429 Discovey looks to be a better match based on price. :)

Since the STM32F429 Discovey uses the STM32F429 and not the STM32F437VIT6 what will be needed to compile for the STM32F437VIT6 after having a project setup for the STM32F429 Discovey?

For example if I am using something like Atollic will a single project for the  STM32F429 and then update the same project to use the  STM32F437VIT6 will this be straight forward?

Thank you for your thoughts.

-Mike