STM32F429: USB Custom Class
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-12-23 12:39 AM
Posted on December 23, 2014 at 09:39
Hello everyone,
Im having problems to implement a USB custom class , using the eval board ''STM324x9I-EVAL'' . Im new in STM32, so any help will be appreciated. The device is recognized by the PC Host as an unknown device. I want to know if the problem is on my configuration or what im missing. Development Enviroment:Tool Version Numbers:Toolchain: MDK-Lite Version: 5.12.0.0Toolchain Path: C:\Keil_v5\ARM\ARMCC\BinC Compiler: Armcc.exe V5.05 (build 41)Assembler: Armasm.exe V5.05 (build 41)Linker/Locator: ArmLink.exe V5.05 (build 41)Library Manager: ArmAr.exe V5.05 (build 41)Hex Converter: FromElf.exe V5.05 (build 41)CPU DLL: SARMCM3.DLL V5.12.0.0Dialog DLL: DCM.DLL V1.13.0.0Target DLL: UL2CM3.DLL V1.153.0.0Dialog DLL: TCM.DLL V1.14.2.0Im performing this on the main: p = USBD_Initialize(0); if(p == usbOK) p = USBD_Connect(0);Also, any document or tutorial on how to use, the USB library would be appreciated.Best Regards,
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0