cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32F207ZG New fragment overlaps old data (retransmission?)

ezrab
Associate II
Posted on December 23, 2014 at 07:28

hi.

i am working with stm32f207zg ang KSZ8051RNL in RMII i used the web server example with the lwip on it and change the phy register 

accordingly

and tested it i am getting alot of error in packages i test it with wireshark after severel refreshes i get New fragment overlaps old data (retransmission?) that repeats severel times and then stops.

these are my defenitions:

  EthHandle.Instance = ETH;  

  EthHandle.Init.MACAddr = macaddress;

  EthHandle.Init.AutoNegotiation = ETH_AUTONEGOTIATION_ENABLE;

  EthHandle.Init.Speed = ETH_SPEED_100M;

  EthHandle.Init.DuplexMode = ETH_MODE_FULLDUPLEX;

  EthHandle.Init.MediaInterface = ETH_MEDIA_INTERFACE_RMII;

  EthHandle.Init.RxMode = ETH_RXPOLLING_MODE;

  EthHandle.Init.ChecksumMode = ETH_CHECKSUM_BY_HARDWARE;

  EthHandle.Init.PhyAddress = 0x01;

i can also see that register ETH_DMAMFDOCR value always increase in time.

i realy need your help here.

thanks.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0