cancel
Showing results for 
Search instead for 
Did you mean: 

Linker file error

rajivpatil61
Associate II
Posted on December 23, 2014 at 10:40

I am trying to build a program at a different location of flash, I am assigning the memory of flash at 0x08020000(by default it will be at 0x08000000). during build time, it pops multiple errors like this

lkarm E112: cannot locate 1 section(s):

lkarm I455:   requirement: 0x4 bytes of ROM area in space ARM:ARM:linear

lkarm I456:   section type: absolute restriction - at address 0x8000184

lkarm I457:   _vector_97 (122) (0x4 bytes)

what is the problem?? PLease Help
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0