2016-06-08 4:09 AM
Hi all,
I am trying to read the onboard Gyro on STM32F4 discovery board. As mentioned in datasheets, Gyro(L3GD20) is conneted to SPI 5. I have configured everything, but I am not able to generate the required clock on SCK pin.SPI 5 SCK,MISO,MOSI and CS pins are - PF7,PF8,PF9,PC1 as per schematic. Because of this I thnik, I am not able to recive byte from SPI on my UART.Pls help...Thanks ...void L3GD_CS_init(void){ RCC->AHB1ENR |= (RCC_AHB1ENR_GPIOCEN); GPIOC->MODER |= 0x00000004; //PC1 as O/P GPIOC->OSPEEDR |= 0x00; //GPIOC->PUPDR |= 0x00000004; //Pull up PC1 //L3GD20_CS_HIGH;}void Spi_pins_set(void){ //PF6, PF7,PF8,PF9 as NSS,SCK,MISO,MOSI...refer to schmeatic for L3GD20 to SPI 5 as AF //PC1 as CS pin for L3GD20...schematic RCC->AHB1ENR |= (RCC_AHB1ENR_GPIOFEN); GPIOF->MODER |= 0x000A8000; GPIOF->OTYPER |= ((uint16_t)0x0000); GPIOF->OSPEEDR |= 0x000A8000; //GPIOF->PUPDR |= 0x00; GPIOF->AFR[0] |= 0x50000000; GPIOF->AFR[1] |= 0x00000055; //AF5 in AFR}void Spi_init(void){ //APB2 has clock 2x slower than processor speed, in my case I have 168MHz core clock, APB2 has 84MHz //APB2 communication bus has 84MHz //And because minimal prescaler for SPI is 2, max frequency is 42MHz //SPI Clock = APBx / prescaler = 84MHz / 2 = 42MHz //By default, prescaler 32 is used: //SPI Clock = APBx / prescaler = 84MHz / 32 = 2.62MHz /* Enable SPI clock */ RCC->APB2ENR |= RCC_APB2ENR_SPI5EN; /* Disable first */ SPI5->CR1 &= ~SPI_CR1_SPE; SPI5->CR1 |= SPI_CR1_BR_0 | SPI_CR1_BR_2 | SPI_CR1_MSTR; //Mode 0 SPI_CR1_LSBFIRST | SPI_CR1_SSM | SPI_CR1_SSI /* Enable SPI */ SPI5->CR1 |= SPI_CR1_SPE;}uint8_t L3GD20_ReadSPI(uint8_t address) { uint8_t data; L3GD20_CS_LOW; /* Send address with read command */ SPI_Send_byte(SPI5, address | 0x80); /* Read data */ data = SPI_Send_byte(SPI5, 0xFF); //L3GD20_CS_HIGH; return data;}int main(void){ uint8_t ch=0; int i=0; SystemInit(); usart1_set(); usart1_init(); Spi_init(); Spi_pins_set(); led_init(); L3GD_CS_init(); while(1) { ch = L3GD20_ReadSPI(L3GD20_REG_WHO_AM_I); //in L3GD20.h file USART1_send_char(ch); USART1_send_char(0x0D); for(i=0;i<5000000;i++); }} #discovery #l3gd20 #stm32f429 #spi #gyroscope2016-06-09 7:05 AM
Hi,
I suggest that you start from CubeMX where you configure your SPI and generate the initialization code. Also, you can refer to the examples under the STM32CubeF4 package, which can help you to develop your application:STM32Cube_FW_F4_V1.12.0\Projects\STM32F4-Discovery\Examples\SPIRegards